Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How the events are managed and stored in the event buffer of BMXNOR0200 Modicon X80 module
Issue:
How the events are managed and stored in the event buffer of BMXNOR0200 Modicon X80 module

Product Line:
BMXNOR0200H

Environment:
All

Resolution:

There are two modes of events storage

1. Store All Events

Here all the events are stored until they reach the limit of storage which can be set by the user.
If still, the events are coming they get lost.

There is one option called " Delete the oldest events "  if selected then the FIFO strategy is implemented in the event buffer. if this is not selected then the additional events are lost.

2. Store only recent events

Here only the recent event for the data point is stored, so if there are 5 events for a single data point
then the fifth event which is the recent one will get stored and all others are deleted