Tìm các câu hỏi thường gặp
What is the latest version of Unity Pro XLS and will it run on Windows 10?
The current version of Modicon Safety Software is for M580 only. It has been renamed and is now called Control Expert v15.0 with the safety option. It is supported on Windows 10.
The last version of Unity XLS was v13.1. It is supported on Windows 10. It will not program Unity Quantum Safety modules, the only supported Safety controllers are M580.
Unity XLS v7.0 is the last Unity Quantum Safety controller programming Software. It only supports Windows XP Pro, 7 32-bit, and 7 64-bit.
The last version of Unity XLS was v13.1. It is supported on Windows 10. It will not program Unity Quantum Safety modules, the only supported Safety controllers are M580.
Unity XLS v7.0 is the last Unity Quantum Safety controller programming Software. It only supports Windows XP Pro, 7 32-bit, and 7 64-bit.
Đã phát hành cho:Schneider Electric Việt Nam
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: