Hôm nay chúng tôi có thể giúp gì cho bạn?

UnityGPL library: if DFB EIOSTESYST can be used under M580 architecture?

Question:
if DFB EIOSTESYST from GPL library can be used under M580 architecture?

Answer:
No, EIOSTESYST DFB do not support corresponding device DTM for M580/M340 controllers