Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How do I disable a logic section in Control Expert (formerly Unity)?

Issue:

How do I disable a logic section in Control Expert (formerly Unity)?

Product Line:

Logic Section, Control Expert, Unity Pro

Resolution:

Step 1: Right click on Section Name in the Browser
Step 2: Select Properties
Step 3: Select the Condition Tab
Step 4: Select a variable name from the Data Editor or create a new variable. When the variable is turned on or off you'll see a green Icon or a red Icon next to the section name indicating the section is solving (green) or its
being disabled (red)


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)