Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What would cause the ATV61 drive mounted inside a MCC to show a PRA drive status only when the HOA is in auto mode?
Issue:
What would cause the ATV61 drive mounted inside a MCC to show a PRA status?

Product Line:
ATV61 MCC

Environment:
All with HOA

Cause:
HOA was miswired PWR input was wired to LI3 auto manual and HOA was wired to PWR input

Resolution:
Troubleshoot this circuit by checking the status of PWR input.  In this case the HOA was wired in error to the PWR input. So the Drive is Rdy in hand and off but goes to PWR when they switch to Auto.
Moved the wire from LI3 to PWR and from PWR to LI3
Now it works.
circuit diagram