Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Power Monitoring Expert - Why are some device types missing from the DeviceType table in ION_Network, such as Micrologic, Sepam, Compact NSX?
Issue
Device types missing from the DeviceType table in ION_Network.

Product Line
Power Monitoring Expert (PME) 8.2 and later
CM2000, CompactNSX A/E, DM6200, DM6300, EM5600, Micrologic A/E/H/P, Momentum PLC A8 WAGES/D10 WAGES
PM600, SEPAM 10/20/40/48/60/80, VIGILOHM, TWIDO_MOD_PLC_WAGES_D12_D28_D44, PM9C, PM1200

Environment
Power Monitoring Expert (PME) 8.2 and later

Cause
The ION_Network database has been deleted and has been recreated using the PME Installer in Reconfigure mode.
If this has been done, the following device types will not get added to the system:

CM2000
CompactNSX A/E
DM6200
DM6300
EM5600
Micrologic A/E/H/P
Momentum PLC A8 WAGES/D10 WAGES
PM600
SEPAM 10/20/40/48/60/80
VIGILOHM
TWIDO_MOD_PLC_WAGES_D12_D28_D44
PM9C
PM1200

Resolution
*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio.
Databases should be backed up prior to performing any procedure.*


To add these device types into the system, open SQL Server Management Studio and execute the SQL script file named 'PME-DeviceDrivers.sql' within a SQL Query window.
This file is found in the <INSTALL DIR>\system\etc\Database\network directory. Running this script will add the missing device types.

Note: It is only the device type definitions in the DeviceType table in ION_Network that are missing. All other supporting files (Vista diagrams/driver files) will be there as expected.