Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What is the difference between the M580 PAC BMEXBP backplane's two types of connectors, Ethernet and X Bus?

Article available in these languages: Tiếng Tây Ban Nha

Issue
The difference between the M580 PAC BMEXBP backplane's two types of connectors, Ethernet and X Bus

Product Line
Modicon M580 PAC BMEXBP

Environment:
EcoStruxure Control Expert
Unity Pro

Resolution
The Modicon M580 PAC BMEXBP backplanes have two types of connectors, Ethernet and X Bus.
The X Bus connection present on all M580 racks is the vary same that is used on the M340 backplane.
It is used for to obtain and exchange the below type of data with the M580 CPU:
1.  Configuration data for the X80 modules
2.  Application and diagnostic data

The BMEXBP backplane Ethernet connector is used for:
1. eX80 I/O modules, which require an Ethernet bus on the rack in order to exchange data (for example, X80 HART modules)
2. Communications to third-party modules that require Ethernet
3. Ethernet communication modules that interlink to the M580 CPU

On the BMEXBP Backplanes, the Slot positions with only 1 connector are used ONLY for XBUS communications. Ethernet Communication and Expert Modules can NOT use these slots,
The Slot positions on the BMEXBP backplanes when 2 connectors use both the XBUS and Ethernet Backplanes. Ethernet Communication and Expert Modules MUST ONLY use these slot types.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)