Product Line
PM3255
Environment
Installation and commissioning.
Resolution
The power meter provides multi-tariff energy accumulation. It supports up to 4 tariffs.
The tariff switching has the following 3 kinds of control modes:
• Digital input
• Communication
• Internal real-time clock (RTC)
Đã phát hành cho: Schneider Electric Việt Nam