Hôm nay chúng tôi có thể giúp gì cho bạn?

How many explicit requests to X80 NOM are supported per one CPU scan

For Quantum and M340, it is 16 requests per CPU scan.
For M580, BMEH582040 is 32 requests per CPU scan
BMEH584040 is 80 requests per CPU scan
BMEH586040 is
96 requests per CPU scan