Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Reading status of the LED diodes LNK, MS on Altivar Process ATV600 or the LED diodes state on VW3A3720 or VW3A3721 Ethernet communication cards by Modbus or by any other communication?

There is no register in Altivar that mirrors the state of LED diodes on Altivar process front panel or the state of LED diodes on VW3A3720 and VW3A3721 communication option card.

The information about the ethernet communication is stored in Altivar in different form.
1. There is possibility to monitor ethernet traffic using Altivar DTM library - see section Diagnostic. You will find there:
- MAC address
- Counter for OK frames received
- Counter for OK frames transmitted
- number of open connections
- number of modbus messages received and transmitted
- number of modbus errors
- and FDR related diagnostic.
2. There is possibility to get information via web server, especially
- active connections with port number, number of transmitted and received OK frames, number of errors
- link and speed on port1, link and speed on port2.
3. Diagnostic on ethernet can be accessible via HMI as well. You can get more-or-less the same data as mentioned above.

When it comes to Ecostruxure control expert, if the Altivar process drive has been added via its DTM into Ecostruxure control expert you will be able to monitor data as mentioned in (1). These data also exists in Altivar registers, but they are not available for users.
LED diodes on Altivar process front panel or on VW3A3720 and VW3A3721 are used for diagnostic on ethernet data link layer. This layer is very close to physical medium and helps to identify whether ethernet connection has been successfully negotiated (speed, half/full duplex) between Altivar and nearest communication port (switch, router, server, PLC, etc.)