Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to Find the Owner of a Shared Power Monitoring Expert (PME) Trend
Issue
Would like to find who is the owner of a particular saved and shared Power Monitoring Expert (PME) trend.

Product
Power Monitoring Expert 8.x

Environment
SQL Server Management Studio

Cause
There is currently no method to find out who owns a particular saved trend within the User Interface of Power Monitoring Expert (PME).
Typically, only the owner of the trend can modify it.  Therefore, in order to make any desired changes to it, the owner would need to be identified.

Resolution
*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio.
Databases should be backed up prior to performing this procedure.*


The following SQL query will return configuration information for a particular saved trend with the UserId of the owner displayed in the UserId column.
Execute the following query in a New Query window within SQL Management Studio, replacing '%TRENDNAMEHERE%' with the name of the trend to be retrieved.

SELECT *
FROM [ApplicationModules].[Configuration].[ConfigurationSettings]
WHERE
Item = 'Realtime Trend'
And Value LIKE '%TRENDNAMEHERE%'

-- Example
SELECT *
FROM [ApplicationModules].[Configuration].[ConfigurationSettings]
WHERE
Item = 'Realtime Trend'
And Value LIKE '%Keating Energy%'

Schneider Electric Việt Nam

Phần đính kèm
TrendQuery.sql [141 Bytes]
Tìm hiểu thêm
Sản phẩm:
Tìm hiểu thêm
Sản phẩm: