Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to generate SQL database detail Disk Usage report?
Issue
How to generate SQL database detail Disk Usage report?

Product Line
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0+
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023


Environment
SQL server databases

Resolution
Display data and log space information for a database

** Warning:  Only those familiar with SQL server and PME should be working with SQL Management Studio.  Making direct modifications to the PME databases can leave a system inoperable and require restoration from back ups. **

1)  Log in to SQL Management Studio
2)  Expand the databases folder, right click ION_Data, select Reports < Standard Reports <  'Disk Usage'
SSMS Disk Usage

3)  To export the report, right click anywhere on the report and select Export and select Excel, PDF or Word

SSMS Disk Usage Report