Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Data Center Expert | How do I configure the location of my advanced view installation for launching to NetBotz Appliances?
Issue:
When attempting to launch Advanced View within Data Center Expert, an error occurs stating that “You must configure the location of your Advanced View installation in Client Preferences to use this feature.”

Product Line:
Struxureware Data Center Expert (DCE)

Environment:
Struxureware Data Center Expert (all verisons)

Cause:
The location of the Advanced View installation has not been configured (or configured incorrectly) in the Data Center Expert desktop client.

Resolution:
  1. Log into the Data Center Expert desktop client.
  2. File menu > Client Preferences.
  3. Select Advanced View Settings.
  4. Select Browse and navigate to the Advanced View executable within Advanced View's installation directory.
  5. Click Apply and OK.