Hôm nay chúng tôi có thể giúp gì cho bạn?

What’s the maximum number of words for data out flow variables in BMENOP0300 module?

Question: What’s the maximum number of words for data out flow variables in BMENOP0300 module?
Answer: 4000 words. The maximum number of variables depends on the data types included in the application because the lengths of different data types varies. The maximum number of output words includes the sum of client and server output words.