Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to start with a very first new Safety M580 CPU into a Safety configuration ?
When RIO is in the configuration and before to start a new configuration, user has to :
1/ Set the date and time into the PLC , CPU out of the final destinated rack ,
2/ Set an NTP server into the configuration (either external server or CPU as NTP server),
3/ Place CPU into the rack to be used and start the configuration,
4/ Make sure all configured safety I/O modules are unlocked ( eventually, use the top blue button to unlock the locked module )


Reminder : it is required to set the date and time into the PLC in order to have a reliable safe communication between CPU and safety IOs module.

If the configuration with Safety I/Os have been started before the configuration of the time into the CPU,  a synchronization of the time between IOs and CPU is necessary either by :

  • 1: forcing the time using %SW128 see the FA333333 how to proceed
  • 2: downloading again the application into the PLC
  • 3 : doing a power cycle of the entire configuration (CPU AND IOs safety modules)

Schneider Electric Việt Nam

Tìm hiểu thêm
Danh mục:
Tìm hiểu thêm
Danh mục: