Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Why doesn't the BMXAMO0410 report a channel fault in an open circuit condition?

Issue:

Why doesn't the BMXAMO0410 report a channel fault in an open circuit condition?

Product Line:

BMXAMO0410

Resolution:

One common reason is that the "Wiring CTRL" option box for the specific channel has not been selected. If the option is not selected the Channel Fault bit will not sense for open loop. (open ckt).
The ability to detect a broken wire (open circuit) condition is limited to current outputs. The selection is made in the BMXAMO410 configuration screen.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)