Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Is it possible to power the ATV630 or ATV930 drive with an external +24VDC power supply?
Issue:
Is it possible to power the ATV630 or ATV930 drive with an external +24VDC power supply?

Product Line:
Variable Frequency Drives

Environment:
Applies to ATV630, ATV930

Cause:
Need to power the electronics of the drive from a separate external +24Vdc source in the panel

Resolution:
Yes, use an external 24Vdc power supply and wire it to "P24" and "0V" terminals on the ATV630 and ATV930.

Note: You cannot run a drive with only 24VDC provided. Use an external 24V only to power the electronics of the drive for programming purposes.