Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Where can I find information on ATV630 maximum inrush current ratings?
Issue:
Looking for information on ATV630 maximum inrush current ratings?

Product Line:
Altivar 630 ATV630

Environment:
All

Cause:
Would like to know the maximum inrush current ratings of the ATV630 to match a drive to a spec

Resolution:
Information tables listing the maximum inrush current ratings are located in the ATV630/650 Installation Manual in section 2.3 Electrical Data, which starts on page 58. The drives' ratings are listed for normal duty and heavy duty. The Installation Manual can be downloaded from here: https://www.se.com/ww/en/download/document/EAV64301/