Hôm nay chúng tôi có thể giúp gì cho bạn?

ATV600 ATV900 how can I find hidden or missing parameters?

Issue:
hidden or missing parameters on ATV Process Drives

Product Line:
Altivar Process ATV930, ATV950, ATV630

Environment:
ALL

Cause:
When I enter on a menu header parameters are missing

Resolution:
If parameters are not visible in some of the menus
First you need to verify under My Preferences > Parameter Access > Visibility is set to "ALL"
Under My Preferences > Access Level is "Expert"
Now, if you still have missing parameters in some of the menus they may have been intentionally hidden.
Go to My Preferences > Parameter Access > Restricted Access > Restricted Param. > and press the button under "None" on any with check boxes checked.