Maximum recording time depends on configuration; number of channels set to be recorded and sampling rate for the recordings. If the recording time for one record is shorter than maximum time the device will have more buffers. Maximum number of buffers is 12.
Đã phát hành cho: Schneider Electric Việt Nam