Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Why is there no serial cable included with my new Smart-UPS SRT5kVA -10kVA

Issue:

Serial cables are no longer included with Smart-UPS SRT5kVA - 10kVA Models

Product Line:

Smart-UPS SRT

Environment:
SRT5KRMXLI, SRT5KRMXLIM, SRT5KRMXLT, SRT5KRMXLT-IEC, SRT5KRMXLW-HW, SRT5KXLI, SRT5KXLT, SRT5KXLT-IEC
SRT6KRMXLI, SRT6KRMXLIM, SRT6KRMXLT, SRT6KRMXLT-IEC, SRT6KXLI, SRT6KXLT, XRT6KXLT-IEC
SRT8KRMXLI, SRT8KRMXLIM, SRT8KRMXLT, SRT8KRMXLT-IEC, SRT8KXLI, SRT8KXLT, SRT8KXLT-IEC
SRT10KRMXLI, SRT10KRMXLIM, SRT10KRMXLT, SRT10RMKXLT-IEC, SRT10KXLI, SRT10KXLT, SRT10KXLT-IEC,

Cause:

Due to the continued decline and elimination of serial communication ports in server manufacturing and to minimize e-waste, APC™ by Schneider Electric will no longer be providing the RJ-45 to serial communication cable with the above Smart-UPS™ models

Resolution:
A serial cable can be ordered free of charge by contacting the Customer Care Centre using https://www.apc.com/us/en/support/contact-us/ .
You will need your exact model and serial number available when registering. You can find this information on the back of the UPS, a sticker on the corner of the shipping box, or via the "About" menu on the LCD screen.