Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What is the meaning of the Max switch-on time parameter valid for an external braking resistor connected to the Servo drive Lexium LXM32
Resext_on, the max permissible switch-on time for external braking resistor is max continuous period for current delivered to external braking resistor. After this time at the latest, there must be a "pause" inserted. During the pause, no current is delivered to the braking resistor. The purpose is to balance resistor temperature and to avoid a high rise of temperature followed by long fall (cooling during pause).
The parameter should not be greater than 10% of the resistor time constant.
On the other hand, the parameter should not be very small as it can limit the current delivery and braking dynamics for high inertia loads.