Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How can I obtain schematics for the AC Drive power board?
Issue:
Is there a way to obtain Schematics for a Schneider Electric AC Drive power board?

Product Line:
Altivar AC Drives, Process Drives

Environment:
All

Cause:
Repair

Resolution:
Drive Products Support does not provide that level of information to the public.  It is internal, proprietary information.  The Schneider Electric Repair Depot does board level repairs, however, typically smaller drives, repair is not very cost effective, and they should simply replaced if/when needed.
The Schneider Electric Repair Depot can be contacted by calling 800-950-9550, more information is available here: Contact Us - Schneider Electric (schneiderelectricrepair.com).

Schneider Electric Việt Nam

Tìm hiểu thêm
Danh mục:
Tìm hiểu thêm
Danh mục: