Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What are Schneider electric products affected by the spectre and meltdown?
Issue

What are Schneider electric products affected by the spectre and meltdown?

Product Line

M580

Resolution

Schneider Electric has become aware of two side channel attacks that leverage critical vulnerabilities in a wide range of computer CPU. These vulnerabilities have been named Spectre and Meltdown. Spectre tricks other applications into accessing arbitrary locations in their memory. Meltdown breaks the mechanism that keeps applications from accessing arbitrary system memory. There have been no known exploits in the wild.
In Schneider Electric product portfolio, only the Modicon M580 uses a vulnerable processor.
Other products are not impacted.
More information at the below link


https://www.se.com/ww/en/download/document/SEVD-2018-005-01/