Hôm nay chúng tôi có thể giúp gì cho bạn?

Data expected behavior on SAVE_DATA and RESTORE_DATA depending the Unity Pro version.

>>Official expected behavior:
Unlocated and located data have the same behavior and It is possible to do a SAVE_DATA even if there are data forced.
Will be implemented on Unity Pro V13.1
VariableValue when “Save Data”Values just before “Restore Data”Expected Value after “Restore Data”Comments
MyM100010Value SAVE
MyM1010F1F1Forced status before RESTORE
MyUnloc1010Value SAVE
MyUnloc20F1F1Forced status before RESTORE
MyM100F101Value SAVE but unforced
MyM101F1F0F0Forced status before RESTORE
MyUnloc1F101Value SAVE but unforced
MyUnloc2F1F0F0Forced status before RESTORE
NOTA: No Red Forced Bit status in status Bar

>> Behavior with Unity Pro V12.0 and V13.0
To solve an issue reported on Up V11.1 it was decided do not save data with forced bit.
VariableValue when “Save Data”Values just before “Restore Data”Values just after “Restore Data”Comments
MyM100010Value SAVE
MyM1010F1F1Value before RESTORE
MyUnloc1010Value SAVE
MyUnloc20F10Value SAVE (*)
MyM1001
MyM101F1
MyUnloc11
MyUnloc2F1
(*) Red Forced Bit status in status Bar (not expected, value being not forced)

>>Behavior with Unity Pro V11.1 and previous version.
VariableValue when “Save Data”Values just before “Restore Data”Values just after “Restore Data”Comments
MyM100010Value SAVE
MyM1010F1F1Value before RESTORE
MyUnloc1010Value SAVE
MyUnloc20F10Value SAVE (1)
MyM100F101Value SAVE
MyM101F1F0F0Value before RESTORE
MyUnloc1F10F1Value SAVE (2)
MyUnloc2F1F0F1Value SAVE
(1) Red Forced Bit status in status Bar (not expected, value being not forced), can be change on INIT
(2) No Red Forced Bit status in status Bar (not expected, value being forced), can be changing the item from unforced to Forced.

NOTA: Possibility to force unlocated data is possible since Unity Pro V8.0 and M580 offer.
NOTA: Working with Unity Pro in simulation mode doesn’t allow to force unlocated data.