Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
S-flex runs in BYPASS mode, but will not run in AFC mode.

Issue:
S-flex not running in AFC

Product Line:
S-Flex


Resolution:
Verify that the ATV212 is in Remote mode, not Local mode.
Verify the VFD has a speed reference.  It may be running at 0Hz.
Verify operation of the DOC contactor and control power to the coil.
Check for loose connections.
Look for control component failure based on the wiring diagram and expected action.

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.