It is possible to configure fallback function. It is the speed that will be applied to the motor when communication is lost.
How to configure it?
For modbus RTU communication :
In fieldbus monitoring set SLL=fallback speed and LFF=xx Hz (fallback speed).
Modbus timeout is set in parameter TTO
For embedded ethernet (ATV340...E) :
ETHL = fallback speed, LFF = xx Hz (fallback speed)
For other type of communication search associated setting in Somove software, in section : Error / warning handling - Communication module
or via VW3A1111 keypad connected to ATV340, search associated setting in the same section Error / warning handling - Communication module
Đã phát hành cho: Schneider Electric Việt Nam