Are there instructions available showing how to install NetShelter seismic mounting brackets onto different floor types?
Issue:
The NetShelter seismic mounting brackets need to be mounted to the floor. There are different floor types.

Product Line:
NetShelter SX

Environment:
All models, all serial numbers.

Cause:
The NetShelter seismic mounting brackets installation manuals only show mounting to the cabinet, not the floor.

Resolution:
Using the pallet bracket or AR7701 the NetShelter SX can be installed per IBC Low Seismic Area and Moderate Seismic Area onto a concrete slab, concrete fill over metal deck, raised composite floor concrete filled metal deck, and raised composite floor concrete slab.
Reference the IBC Seismic Calculations for NetShelter SX for instructions: http://www.apc.com/salestools/SNEL-8C7UQS/SNEL-8C7UQS_R6_EN.pdf
An updated document can be loaded off the APC website of any NetShelter SX cabinet under the Documentation tab.

Using AR7701A-S the NetShelter SX can be installed per OSHPD onto a concrete slab, and concrete fill over metal deck.
Reference the OSHPD structural drawings for NetShelter SX for instructions: http://www.apc.com/salestools/JKUR-ATJL8V/JKUR-ATJL8V_R0_EN.pdf
The AR7701A-S can also be installed to meet IBC High Seismic Area using these instructions:
http://www.apc.com/salestools/SNEL-8C7UQS/SNEL-8C7UQS_R6_EN.pdf


Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: