Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Video: How to generate a Meter Configuration report using ION Setup

Article available in these languages: Tiếng Tây Ban Nha

Issue
User may need to generate a Meter Configuration report or Event Log in ION Setup

Product Line
PowerLogic Power Meters
ION Power Meter

Environment
ION Setup

Resolution
For ION Meters:
  1. Select the desired ION Meter
  2. Double-click on Setup Assistant to launch Setup Assistant
  3. Select Reports
  4. To generate a Meter Configuration report, double-click on Meter Configuration
    • To save the file in text format, click Save As...
    • Select a file location, type desired file name, and click Save


For PowerLogic Meters
  1. Select the desired PowerLogic Meter
  2. Double-click on Reports
  3. To generate a Meter Configuration report, select Meter Configuration and then click Display
    • To save the file in text format, click Save As...
    • Select a file location, type desired file name, and click Save