Does the ATV930 have Torque Limitation and is an input assignment required to activate it?
Issue:
Does the Process Drives have Torque Limitation and do you have to assign an input?

Product Line:
ATV900

Environment:
All

Cause:
Wiring

Resolution:
The ATV900 series drives do have the Torque Limitation feature.  It is found in Complete Settings > Generic Functions > Torque Limitation and can either be set to YES for always active or assigned to a digital input for activation.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: