Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Can I use an LTMR Tesys T product to convert between Ethernet IP and Modbus RTU?
Issue:
Customer has an Ethernet IP control network and a device that will communicate Modbus RTU only.  They want to use the Tesys T as a protocol bridge to control the Modbus RTU device.

Product Line:
Tesys T LTMR product.

Environment:
All Ethernet modes, All serial numbers.

Cause:
No information on this configuration available in current literature.

Resolution:
It is not recommended.  Portions of this configuration may work but some portions may not.   This has not been tested for compatibility or reliability and cannot be recommended.  A dedicated Protocol Bridge should be used in this situation.