Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How can I import/export DTM from BMENOC03x1 on Unity Pro 13.1?
Issue
This new feature has been introduced on Unity Pro v13.1 and allow to import a BMENOC0321 or a BMENOC0301/11 module configuration and all the devices configured behind the NOC master DTM.

Product Line
Unity Pro, M580, BMENOC0301, BMENOC0311, BMENOC0321

Environment
Unity Pro 13.1, BMEP584040 v2.80, BMENOC0301 v2.15

Resolution
This is a new feature and some customer are not familiar about how to do it. So, you can follow the steps bellow to import the DTM configuration.
  • Export the module with DTM configuration and it will create a .zhw file
DTM and Project Browser
  • Use M580ApplicationUpdate.exe to make a file conversion. This tool is located in the same program directory as Unity Pro software, by default C:\Users\Public\Documents\Schneider Electric\Unity Pro\Extras\M580 Application Update
M580 Application Update file select
  • You can check the compatibility of the file
M580 Application Update
  • Select an empty slot of the M580 main rack and import. E.g., you can import for the same project or for another project
DTM and Project BrowserFile explorer
Unity Pro

P.S.: You cannot import twice (or more) the same exported file (.zhw) in the same application.