Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How does a chilled water actuator work on an ACRC301H to control dew point after a power loss?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
How does a chilled water actuator work on an ACRC301H to control dew point after a power loss?

Product line:
ACRC301H.

Environment:
All Serial Numbers.

Cause:
Install, Repair.

Resolution

The actuator is a spring return, which means it will close on a power failure or any loss of power.
Upon restart, the fans start first to allow the sensors some time to recognize the air temperature and humidity as well as the fluid temperatures. The CW valve opens very slowly and monitors the coil temperature. The valve opening and pump starting is slow enough to catch any excessive changes in temperature and react appropriately. Even if there is a sharp change in temperature of the coil, it will only result in some surface condensation and not be enough to drip from the coil. Any condensate that forms on the coil, once the coil goes above dew point, will evaporate in the air stream.

We can only assure them that this control strategy has been tested thoroughly and will react to avoid condensation.