Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How the DC injection braking is setup on the ATV61/71 drives? What are the Name of parameters included?
Hello,

The setting of DC injection breaking is done through below parameters in menu "Stop Configuration"
- Stt [Type of stop] = [DC injection] (dCI): DC injection stop ---> when you apply stop command the DC injection braking is active.

- dCI [DC injection assign.] = LI1 to LIx ---> The DC Breaking is activated when you give this assigned Logic input LIx - When you apply this logic input (if assigned) it will apply DC injection breaking.

- the below parameters will decide the level of DC current and time, to be fine tuned depending upon the application and load.
- IDC ([DC inject. level 1]
- tdI [DC injection time 1]
- IdC2 [DC inject. level 2]
- tdC[DC injection time 2]

Please refer the programming manual extract for detailed understanding of each parameter setting.

Schneider Electric Việt Nam

Phần đính kèm
ATV71-ATV61 DC injection Braking.pdf [108.18 KB]