Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
With only 3 logic/digital inputs, can you use 2 preset speeds with the S-Flex Altivar 212?

Issue:
With only F, R and RES terminals, can you use 2-preset speeds with the S-Flex Altivar 212?

Product Line:
Altivar Machines, Altivar 212, S-Flex

Environment:
All models and serial numbers

Cause:
Wiring / Programming

Resolution:
This can be accomplished by programming VIA to function as a Logic input, as follows:
Press Mode to AUF (Quick Menu) Enter, scroll down and set LL (Low Limit) to your 1st preset
Mode back to AUF - scroll down to F - - - (Extended Menu) and press Enter
F109 = 2 (assigns VIA as a logic input)
F118 = 6 (assigns the preset speed function to VIA)
Mode back to AUF, scroll down to
SR1.. Enter and set to your desired High/Preset Speed
Close a contact between P24 and VIA to run at high/preset speed, open that contact to run at the LL - Low Speed setting