Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What causes a 4-20mA loss (LFF) on an ATV312 drive?
Issue:
ATV312 4-20mA loss, LFF error code on display

Product Line:
Altivar Machine 312

Resolution:
This will happen if the LFF is programmed to a function other than ignore (no).
If it is programmed to a function other than no, then the drive is designed to have a value of 4 mA minimum (unless CRL3 is changed to 0 instead of 4A) on AI3 input.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)