Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Where can I download version 2.12 DTM file for Tesys T / U products?
Issue:
SoMove does not automatically update to version 2.12 of the Tesys T/U DTM file when "update catalog" is selected from within SoMove.

Product Line:
IEC Contactors and starters

Environment:
Tesys T / U devices, SoMove.Environment:Problem occurs with newer firmware devices that require DTM version 2.10

Cause:
SoMove does not automatically update to DTM version 2.10, manual update is necessary.

Resolution
:The link below will take you to the website where DTM Version 2.10 can be downloaded.  After download, insure that SoMove is not open and running.  Run the Executable file to install the new DTM and then load SoMove and select "Update catalog".  This will load the latest version of the DTM file.

https://www.se.com/ww/en/download/document/TeSysDTMLibrary/