Hôm nay chúng tôi có thể giúp gì cho bạn?

Why is the text on my SBP3000 upside down?

Product Line: SBP3000

Cause: The artwork is correct. The SBP3000 is intended to be wall mounted or used in tower format.

Resolution: The SBP3000 can be rack mounted but it will have the artwork text upside down, unless the bypass panel is oriented with the AC input on the right and switch on the left.

Schneider Electric Việt Nam

Phần đính kèm
SBP3000.png [29.88 KB]