Issue:
Checking on the ZCT limit switch body's available plungers.
Product Line:
Osisense Limit Switches Metal and Plastic.
Environment:
ZCT Limit switch body
Resolution:
Available plungers are ZCE21, ZCE27, ZCE28, ZCE24, ZCE62, ZCE63, ZCE64, ZCE65, ZCE66, ZCEH0, ZCEH2, ZCE02, ZCE29, ZCE10, ZCE11, ZCE13 and ZCE14.
Checking on the ZCT limit switch body's available plungers.
Product Line:
Osisense Limit Switches Metal and Plastic.
Environment:
ZCT Limit switch body
Resolution:
Available plungers are ZCE21, ZCE27, ZCE28, ZCE24, ZCE62, ZCE63, ZCE64, ZCE65, ZCE66, ZCEH0, ZCEH2, ZCE02, ZCE29, ZCE10, ZCE11, ZCE13 and ZCE14.
Đã phát hành cho:Schneider Electric Việt Nam