Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What is Class 5 timing accuracy as described in the Sepam Operation manual?
Issue
User needs clarification of what Sepam class 5 timing accuracy is as a percentage

Product Line
Sepam series 20, 40, and 80

Environment
Accuracy specifications

Resolution
Class 5 accuracy is defined in the IEC 60255-151 standard. Class 5 accuracy is ±5%.

This 5% has factors to be considered referring to different parts of the IDMT curve. These factors are defined in part 5.2(Accuracy related to the operate time) table 1 IEC60255-151(2009). This table is provided below.

This table gives the factors for different ranges (Gs= threshold). To determine the real accuracy, multiply the assigned error of 5% by the limiting error from the above table. The assigned error is based on the accuracy class 5 for the Sepam relay. The real accuracy values for each of these ranges is below:
  • For current between 2 to 5, real accuracy would be 2.5*5% = 12.5%
  • For current between 5 to 10, real accuracy would be 1.5*5% = 7.5%
  • For current higher than 10*Gs or 10 times threshold, real accuracy would be 1*5% = 5%