Hôm nay chúng tôi có thể giúp gì cho bạn?

Is there a method that can be used to update all of the DTM's automatically in a Unity application after installing Control Expert 14?

Issue
If I open a Unity application after installing Control Expert,  I get a message that inidicates my DTM's needs to be updated.
Is there a way to automatically update all of the DTM's with just one mouse click.

Product Line
Control Expert 14

Environment
Windows 8, Windows 10


Resolution
There is no method available for automatically updating all of the DTM's after installing Control Expert using 1 mouse click.
The only method available to update the DTM is by using the following steps:
  • Open the Unity application.
  • Open the DTM.
  • Make a minor change to the DTM (i.e., Change the description by adding a space, etc.)
  • Save the Unity application.
  • Go back and delete the minor change
  • Save the application again.

FAQ Applicable Conditions