Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to set the time and date on an iPC running Vijeo Designer Runtime
Issue:
How to set the time and date on an iPC running Vijeo Designer Runtime

Product Line:
Magelis iPC running Vijeo Designer Runtime (all versions)

Resolution:
In order to properly set the time and date within the Vijeo Designer Runtime, you must be sure that the application is launched as Administrator. In other words, right-click on the Vijeo Designer Runtime icon and select "Run as Administrator". If you do not do this, the changes will not take effect. If you require to run the application automatically at login, please create a scheduled Windows Task to launch VIjeo Designer Runtime when a user logs in. Also, ensure to check the check box to run with the highest privileges in the properties of the task.