Hôm nay chúng tôi có thể giúp gì cho bạn?

How to open a Modsoft application with Concept.

Issue
How to open a Modsoft application with Concept.

Product Line
Concept version 2.6

Environment
Windows 7


Resolution
Concept cannot open the Modsoft application directly.  In order to open a Modsoft application in Concept,
it must first be converted using the 'Modsoft Converter' tool.  The Modsoft Converter tool is installed as part of Concept and it can be found
in the list of program items for Concept within the 'Windows Start\All Programs' menu.

The following steps can be used to open a Modsoft application with Concept:

  • Click on Start
  • Select 'All Programs'.

zxcvb


  • Select 'Concept V2.6 XL EN'.
  • Select 'Modsoft Converter'.

fzgx


  • Click on 'File'.
  • Select '\Convert'.

dfgh



  • Browse for the Modsoft application '.env' filename and select it.
  • Click on 'OK'.

saDfg



  • The 'Modsoft Convert' window will show the application being converted.

dfg


  • Click on 'File'.
  • Select 'Save As'.

sdvfbg

  • Browse for a folder to save the application.
  • Type in name for the Concept application.
  • Click on OK.

vfg



  • Close 'Modsoft Convert'.
  • Start Concept.
  • Open the saved application.

cvfgh

​