Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What is the dissipated heat rating for ATV930 drives?
Issue:
Dissipated heat rating for ATV930 drives.

Product Line:
Altivar 930

Environment:
All

Cause:
Heat loss

Resolution:
Dissipated Heat Ratings

The first value is the power dissipated at a nominal current in the forced-cooled area of the drive.  The second value is the power dissipated at nominal current in the naturally cooled area, the value used in case of installation using the flush-mounting kit, separate hot and control part in the cabinet.  If the drive is installed in a standard cabinet, the sum of both values is to be taken into account.