Issue:
DI1 assignment in IO Map saying not assigned for both DI1 low or DI1 high.
Product Line:
ATV600, ATV900
Environment:
All
Cause:
Customer checked DI1 assignment in I/O Map but didn't see DI1 current assignment 'Forward'.
Resolution:
Check menu 5.5 (Command and Reference), and Control Mode to see if it is set to "I/O profile", DI1 assignment only show "Forward" if the control mode is set to "Not Separate" or "Separate".
Đã phát hành cho: Schneider Electric Việt Nam