Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How does the option "Preload Data Dictionary for online modifications" work in Vijeo Designer?

Issue:
Using "Preload Data Dictionary for online modifications" in Vijeo Designer

Product Line:
EcoStruxure Control Expert(Unity Pro), Vijeo Designer

Environment:
Vijeo Designer

Resolution:
When this option is selected there is a periodic query and retrieval of new unlocated addresses, if they are available. When the PLC’s update timeout expires and the old unlocated addresses become invalid, the
new unlocated addresses will become active with no delay. If this property is disabled, the new unlocated addresses will not be retrieved. You will need to perform a manual update of the symbol file to update and apply the new unlocated addresses.