Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to use LoadDataValue in C#
DISCLAIMER

The example below is intended to demonstrate one or more features or methods and is presented as a configuration example only. Schneider Electric assumes no liability for the use or application of this example or any portion thereof.

LoadDataValue is a method that can be used to insert historic data to a point (more details on the ClearSCADA Database Schema).
Below there is an example on how to connect to a local server and use this method:

private void button9_Click(object sender, EventArgs e)
{
DBObject TestPoint;
Aggregate HistAgg;

Object[] args;
DateTime dt;
args = new Object[4];

using (Connection conn = new Connection("TestApp"))
{
// Connect to local server
SecureString passwd = new SecureString();
string strPassword = "adminexample";
foreach (char c in strPassword)
passwd.AppendChar(c);
passwd.MakeReadOnly();
conn.Connect("localhost");
conn.LogOn("AdminExample", passwd);

// Get the point
TestPoint = conn.GetObject("~Points.A1");
// If Historic is enabled for the point, insert historic data
if (TestPoint.Aggregates.TryGetValue("Historic", out HistAgg) == true)
{
args[0] = 0;
args[1] = 192;
dt = new DateTime(2019, 4, 3, 7, 21, 52);
args[2] = new System.DateTimeOffset(dt);
args[3] = 88;
HistAgg.InvokeMethod("LoadDataValue", args);
}
conn.LogOff();
conn.Disconnect();
}
}