Hôm nay chúng tôi có thể giúp gì cho bạn?

How to create alias array variables using the Unity Excel Tool.

Issue
How to configure a DNP3 array in the BMXNOR0200 using an unlocated array variable.

Product Line
Control Expert

Environment
Windows 7, Windows 10, Windows 8

Resolution
This video will demonstrate how to create a '.xsy' import file that contains unlocated array variables.  Each element of the array variables
are aliased to an unlocated variable.  The export file is created with the Unity Excel Tool named 'Unity Variables Management.xlsm'

https://www.youtube.com/watch?v=SbGKql9bZlo