Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Is there a wiring diagram for the ATV630 / ATV650 Process drives when supplied with single phase power?
Issue:
ATV630/650 Process wiring diagram for single phase power

Product Line:
ATV630 ATV650

Environment:
Models with single phase ratings

Cause:
Requesting wiring diagram

Resolution:
There is no published document that includes a wiring diagram for single phase supply.  Note that the power can be connected in any combination:
L1 / L2
L1 / L3
L2 / L3

Note that for single phase supply, the input phase loss feature needs to be disabled.
Complete settings - Error/Warning handling - Input phase loss = Ignore

PLEASE note that the approved use of ATV630/650 drives for single phase input to run 3 phase motors is very limited.   See this knowledge article for detail: https://www.se.com/eg/en/faqs/FA279836/

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)