Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to flash the firmware of the LXM28 drive
Issue:
How to flash the firmware of the LXM28 drive

Product Line:
LXM28
Lexium 28

Resolution:
To flash the LXM28 drive firmware, the following are needed:
- Latest firmware file (currently V1.70.8). This is a file with the extension *.i00 and can be requested from technical support.
- Firmware Update Tool (latest version is 1.0.2.8) and can also be requested from technical support
- USB to RJ45 cable, part # TCSMCNAM3M002P

> Power the LXM28 drive
>
Connect the USB-RJ45 cable
> Launch the Firmware Update Tool
> Enter the COM port assigned by Windows to the cable
> Browse the firmware in the "Firmware Path"
> Click on Connect - If successful, this should bring up the drive model and version
> Click on Start and wait

The Flash tool is attached herewith.

Schneider Electric Việt Nam

Phần đính kèm
Fw Update Tool_1028.zip [188.79 KB]